October 25, 2012 – Mouser Electronics, Inc. today announced it is taking orders for the new Arduino Due Microcontroller Board from Arduino, based on the Atmel SAM3X8E ARM Cortex-M3 MCU.
The long-awaited Arduino Due Microcontroller Board is based on the 32-bit processor Atmel SAM3X8E ARM Cortex-M3 MCU, and improves all the standard Arduino functionalities, adding many new features. The Arduino Due offers 54 digital input/output pins (of which 16 can be used as PWM outputs, with selectable resolution), 12 analog inputs with 12 bits of resolution, 4 UARTs, two DAC outputs, an 84MHz crystal oscillator, two USB connections, a power jack, an ICSP header, a JTAG header, and a reset button. The maximum voltage that the I/O pins can provide or tolerate is 3.3V. The board has two micro USB connectors—one for debugging purposes and a second one capable of acting as a USB host, allowing external USB peripherals such as mouse, keyboards, smartphones, etc. to be connected to the Arduino Due. This exciting new addition to the Arduino family is now available for order, so visit http://www.mouser.com/arduino-due/ to place your order now.
With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 19 global support locations and the latest, most technologically advanced components for their newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 3 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser
Mouser Electronics, a subsidiary of TTI, Inc., is part of Warren Buffett's Berkshire Hathaway family of companies. Mouser is an award-winning authorized semiconductor and electronic component distributor, focused on the rapid introduction of new products and technologies to electronic design engineers and buyers. Mouser.com features more than 3 million products online from more than 450 manufacturers. Mouser publishes multiple catalogs per year providing designers with up-to-date data on the components now available for the next generation of electronic devices. Mouser ships globally to over 375,000 customers in 170 countries from its 492,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.
About Arduino
Arduino provides open-source electronics prototyping platforms based on flexible, easy-to-use hardware and software. Arduino prototyping platforms are intended for artists, designers, hobbyists, and anyone interested in creating interactive objects or environments. Arduino's prototyping platforms can sense the environment by receiving input from a variety of sensors and can affect their surroundings by controlling lights, motors, and other actuators. Arduino projects can be stand-alone or they can communicate with software running on a computer.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Further information, contact:
Kevin Hess, Mouser Electronics
Vice President Technical Marketing
(817) 804-3833
Kevin.Hess@mouser.com
For press inquiries, contact:
Kelly DeGarmo, Mouser Electronics
Corp. Communications & Media Relations Mgr.
(817) 804-7764
Kelly.DeGarmo@mouser.com